LeakRepair
LeakRepair refers to a pipe that requires, and is scheduled to receive, repair.
Subtypes: None
Associations: LeakReport
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User and designer comments. |
|
DimensionTie1 |
text |
Description of east–west line of feature location. |
|
DimensionTie2 |
text |
Description of north–south line of feature location. |
|
FacilityType |
text |
Code indicating type of facility; examples include Distribution Main, Drip, and Regulator. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
LeakCause |
text |
Code indicating cause of leak; domain values include Construction Defect, Damage – Third Party, Material Failure, etc. |
|
LeakReportObjectID |
long integer |
ObjectID of associated Leak Report. |
|
RepairDate |
date |
Date leak was repaired. |
|
WorkOrderID |
text |
Utility-defined identifier of work order |