Water Field Model Names
|
Model Name |
Object |
|---|---|
|
BONDEDINDICATOR |
The attribute that indicates whether a feature is bonded; if it is bonded, it will not be a barrier to a cathodic protection trace; if it is not, it will be a barrier. Used by water trace solvers. |
|
CPSYSTEMSTATUS |
The attribute that indicates whether or not a feature is a barrier to a cathodic protection trace; used by water trace solvers. |
|
EMERISOLATIONSYSSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the emergency isolation system; used by water trace solvers. |
|
ISOLATIONLEVEL |
Reserved for future use. |
|
MATERIAL |
The attribute on a feature that indicates the material of a feature to determine whether it will be a barrier to a cathodic protection trace; used by water trace solvers. Values: plastic, non-plastic. |
|
NORMALPOSITION |
The attribute on a controllable device (e.g., Valve or Controllable Fitting) that indicates whether the device is open or closed; used by water trace solvers. Values: open, closed. |
|
OPERATINGCLASSIFICATION |
The attribute on a Valve that indicates whether the valve is critical; used by water trace solvers. |
|
OPERATINGPRESSURE |
The attribute on the DistributionMain feature class that indicates the operating pressure of the pipe. |
|
PIPEDIAMETER |
The attribute on a water pipe that indicates its diameter. |
|
PIPETYPE |
The attribute on a water pipe that indicates whether the pipe is a pinchable type; used by water trace solvers. Values: pinchable, non-pinchable. |
|
PIPESTATUSINDICATOR |
The attribute on a water pipe that indicates whether the pipe is pinched or damaged in some way, such that water will not flow through it; used by water trace solvers. Values: open, closed. |
|
SOPIN |
Attribute on RegulatorStation that indicates standard or system operating pressure entering station; used by water trace solvers. |
|
SOPOUT |
Attribute on RegulatorStation that indicates standard or system operating pressure leaving station; used by water trace solvers. |
|
STATUS |
Assign to the Status field on Distribution Main, Valve, Service, and Network Source features; used by water trace solvers. |
|
VALVEUSE |
Reserved for future use. |
|
WATERPRESSURESYSTEMSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the water pressure system; used by water trace solvers. |
|
WATERSYSTEMSTATUS |
The attribute on a feature that indicates whether or not it is a boundary on the water system; used by water trace solvers. |
|
WATERTRACEWEIGHT |
The attribute on all feature classes that represents the trace weight in the geometric network; used by water trace solvers. |