GasStation
GasStation is an abstract class that inherits characteristics from the abstract class GasDevice.
RegulatorStation and TownBorderStation inherit attributes from GasStation.
Gas Stations house and protect pipes and devices that measure and regulate the flow of gas for the purpose of reducing higher pressures to pressures low enough to distribute to customers.
Subtypes: None
Associations: GasStructure, Regulator
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
BypassIndicator |
text |
Indicates whether GasStation is bypassed; domain values include Yes and No. |
|
CPSystemStatus |
text |
Status of associated Cathodic Protection System. |
|
DesignCapacityMCFH |
text |
Maximum amount of gas the station can manage in thousands of cubic feet per hour. |
|
EmerIsolationSysStatus |
text |
Indicates whether feature defines a boundary of Emergency Isolation System; information used for tracing analysis. |
|
GasPressureSystemStatus |
text |
Indicates whether feature defines a boundary of GasPressureSystem. |
|
GasSystemStatus |
text |
Indicates whether feature defines a boundary of GasSystem; information used for tracing analysis. |
|
InsulatedIndicator |
text |
Code indicating whether feature is insulated; domain values are Yes and No. |
|
LocationDescription |
text |
Verbal description of location of the gas station. |
|
MOPIn |
double |
Average maximum operating pressure entering GasStation. |
|
MOPOut |
double |
Average maximum operating pressure leaving GasStation. |
|
Name |
text |
Utility-assigned name of GasStation. |
|
OverPressureProtectionType |
text |
Type of device to prevent overpressuring within system; domain values include Full Capacity Relief Valve, Monitor Only, Operator and Monitor, etc. |
|
PipeDiameter |
text |
Code indicating size of pipe; domain values depend on subtype and include 1/4”, 1/2”, 3”, 40”, etc. |
|
SOPIn |
double |
Average standard operating pressure entering GasStation. |
|
SOPOut |
double |
Average standard operating pressure leaving GasStation. |
|
Status |
text |
Code indicating operating status of GasStation; domain values include Offline, Online, and Unknown. |