StationStructure
StationStructures protect and provide access to above ground gas devices and facilities.
Vault inherits attributes from the GasStructure abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
PipeLineOperator |
text |
Code indicating pipeline operator; examples include American Natural Resources, Midcon, etc. |
|
PipeLineStation |
text |
Pipeline station associated with StationStructure. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on map. |