MainJobSeparator
MainJobSeparator represents the beginning and end points for jobs performed on pipe.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. To support Gas Tracing and Feeder Manager, the model name GASTRACEWEIGHT is required for every feature class belonging to ArcFM gas networks. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
date |
Date pipe set in service. |
|
InstallationDate |
date |
Date of installation. |
|
SubType |
long integer |
Code indicating type of GasPipe; examples include Distribution Main and Service. |
|
SymbolRotation |
double |
Angle that dictates how the feature appears on the map. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |