CPSystem
A CPSystem is composed of multiple pipe sections and defined for the purpose of performing cathodic protection trace analysis.
Subtypes: None
Associations: CPBondWire, CPDevice, GasPipe
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
ID |
text |
Primary key for utility identifier. |
|
ProtectionType |
text |
Type of protection used in system; includes Anode and Rectified.The PROTECTIONTYPE model name is assigned to this field for gas tracing operations. |