Joint Use Attachment
Other utilities or entities may attach conductors or cables that carry signals such as community antenna television systems (CATV) to support structures. Information about owners and joint use attachments is captured in this table. This related object class stores information about a feature with a spatial reference but does not itself have a location on the map.
Structural Analysis (in Designer) uses this object class when performing "what if" simulations to evaluate the structural integrity of a support structure and its associated features.
Subtypes: None
Associations: SupportStructure
Model Names: JOINTUSEATTACHMENT
Attributes:
|
Field Name |
Field Type |
Description |
|
AttachmentDate |
date |
Date object was attached to structure. Uses DATE model name on this field. |
|
AttachmentHeight |
text |
The height of the attachment. This value should be expressed in the same units used for the SupportStructure Height field. |
|
AttachmentType |
text |
The type of attachment. |
|
Chargeable |
text |
A boolean value that indicates whether the attachment is chargeable. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
Owner |
text |
Code indicating owner of attachment; domain values include Cable, Telephone, Other, etc. Structural Analysis uses the JOINTUSEATTACHMENTOWNER model name on this field. |
|
StructureObjectID |
long integer |
Object ID for the structure. |