Device Object
DeviceObject is an abstract class containing common attributes of the devices that control the flow of current in circuits. Device control objects capture characteristic strategies used by regulators and capacitors to provide voltage at a range that allows customers’ equipment to operate properly.
Associations: None
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
FacilityID |
text |
Meaningful company-assigned unique identifier. Many ArcFM tools use the FACILITYID model name on this field. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date device was installed. |
|
Model |
text |
Model of the device. |
|
SerialNumber |
text |
Device serial number. |
|
WorkOrderID |
text |
Work order identifier. |