Aerial Marker
An AerialMarker indicates the presence of overhead cable and structures. AerialMarker inherits attributes from the Structure abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
LightIndicator |
text |
Code indicating presence of light indicator; domain values or Yes and No. |
|
SymbolRotation |
double |
Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features. |