GasStructure
GasStructure is an abstract feature class. GasStructure contains characteristics inherited by Vault and StationStructure that distribute gas to customers.
Subtypes: None
Associations: RegulatorStation, TownBorderStation
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Contractor |
text |
Name of contractor. |
|
FacilityID |
text |
Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
data |
Date device was set in service. |
|
InstallationDate |
date |
Date of installation. |
|
LocationDescription |
text |
Verbal description of location of GasStructure within Facility. |
|
Material |
text |
Material of GasStructure. Domain values include brick, concrete,steel, etc. |
|
Owner |
text |
Owner of GasStructure. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
RegulatorStationObjectID |
long integer |
ObjectID of associated regulator station. |
|
StructureHeight |
text |
Height of GasStructure. |
|
StructureLength |
text |
Length of GasStructure. |
|
StructureWidth |
text |
Width of GasStructure. |
|
TBSObjectID |
long integer |
ObjectID of town border station. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |