CPRectifierCable
A rectifier cable carries power from the gas main to the rectifier and to the anode as part of the cathodic protection system. CPRectifierCable is represented as a complex edge feature because multiple connections to the network are made along its edge.
You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPRectifierCable feature class.
Subtypes: None
Associations: CPAnode
Model Names: GASNONTRACABLE
Attributes:
|
Field Name |
Field Type |
Description |
|
Comments |
text |
User or designer comments. |
|
Depth |
double |
Depth of CPRectifierCable. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. Gas tracing uses the GASTRACEWEIGHT model name on this field. |
|
Gauge |
text |
Code indicating gauge of cable; domain values are 4, 8, and unknown. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InstallationDate |
date |
Date of installation. |
|
LengthSource |
text |
Source of length measurement; domain values are Mapping System and Field Measurement. |
|
MeasuredLength |
double |
Field-measured length of CPSection, ranging from 1 to 1,000,000,000. Gas tracing uses the MEASUREDLENGTH model name on this field. |
|
OperatingStatus |
text |
Code indicating functional status of Rectifier Cable; examples include Active, Designed, and Proposed Retire. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |