Circuit Source ID
This table stores the ultimate sources defined in the CircuitSource object class as well as the subsources defined in a multi-tiered network. This table is required ONLY for Extended Feeder Manager.
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
FeederLevel |
long integer |
A value indicating the feeder level. A feeder level consists of all connected features with the same voltage level. This voltage level is determined by the exiting voltage from a subsource. All connected downstream features with that same voltage are considered a feeder level. |
|
FeederName |
text |
This field contains the name assigned to the feeder. |
|
ParentCircuitSourceID |
long integer |
This field contains a value that identifies the parent circuit source to the electric device. This field is required by Extended Feeder Manager. |
|
RelatedFeatureClassName |
text |
The feature class name for the related object. |
|
RelatedObjectID |
text |
A unique ID that identifies the related object. |