Synchronous Motor
Synchronous motors transform electric power from an alternating current system into mechanical power. The armature winding, usually on the stator, is the current carrying winding. The configuration of the rotor determines the type of synchronous motor and usually employs dc-excited field windings. Synchronous motors are built for operating at a power factor or 1.0 or 0.8 lead. Reactance is measured in a steady-state condition in which a circuit’s values remain essentially constant, occurring after all initial transients or fluctuating conditions have settled down.
Associations: ServicePoint
Subtypes: None
Model Names: SYNCHRONOUSMOTOR
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
ArmatureResistance |
double |
Resistance of armature winding in ohms. |
|
ConnectionConfiguration |
text |
Code indicating connection configuration of SynchronousMotor. |
|
DAxisSynchronousReactance |
double |
Ratio of reactive armature voltage to direct axis reactance under steady-state conditions. |
|
QAxisSynchronousReactance |
double |
Ratio of reactive armature voltage to quadrature axis reactance under steady-state conditions. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
SaturationCoefficient10 |
double |
Saturation coefficient at 1.0 per unit (PU) noterminal voltage. |
|
SaturationCoefficient12 |
double |
Saturation coefficient at 1.2 PU no-terminal voltage. |
|
ServicePointObjectID |
long integer |
ObjectID of ServicePoint. |
|
SubtransientReactance |
double |
Subtransient reactance in ohms. |
|
TransientReactance |
double |
Transient reactance in ohms. |
|
ZeroSequenceReactance |
double |
Ratio of in-phase armature voltage to negative sequence reactance. |