Service Point
ServicePoint is the point at which the distribution feeder terminates and energy is supplied to a customer. A service point can have one or many meters.
Designer Secondary Circuit Analysis requires the SERVICEPOINT model name on this class.
Responder uses the FDRMGRLOADPOINT model name on this class. Future Feeder Manager functionality may take advantage of this model name as well.
Associations: InductionMotor, SynchronousMotor
Subtypes: None
Model Names: SERVICEPOINT, FDRMGRLOADPOINT
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Comments |
text |
User or designer comments. |
|
Status |
text |
Code indicating status of ServicePoint; domain values include Active and Inactive. |