Service Address
Associations: CustomerConnection
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
AccountID |
text |
Unique identifier for the customer's account. |
|
AcctType |
text |
The type of account. |
|
Address1 |
text |
Customer address. |
|
Address2 |
text |
Customer address. |
|
Block |
text |
Block number of the customer's address. |
|
City |
text |
Customer's city. |
|
Comments |
text |
User or designer comments. |
|
CriticalCustomerIndicator |
text |
Code indicating whether customer has critical need for electricity; domain values include Critical, Non-Critical. |
|
CustomerClass |
text |
Code indicating class of customer; domain values include Commercial, Industrial, MultiFamily Residential, and Single Family Residential. |
|
DesignID |
text |
Unique identifier for the design associated with the customer's address. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
LocationID |
text |
Unique identifier for the customer's location. |
|
Lot |
text |
Lot number of the customer's address. |
|
QtrSection |
text |
The number of the quarter section containing the service address (based on the Public Land Survey System). |
|
Range |
text |
The number and direction of the range (parallel to the principal meridian, based on the Public Land Survey System) (e.g. R18E = Range 18 East). |
|
Section_ |
text |
The number of the section within a township (e.g. S10 = Section 10). |
|
Situs |
text |
The jurisdiction where the property is treated as being located for legal purposes. |
|
State |
text |
Customer's state. |
|
StreetDir |
text |
Street direction in the customer's address (e.g., North, South). |
|
StreetName |
text |
Street name in the customer's address. |
|
StreetNo |
text |
Street number in the customer's address. |
|
StreetSuf |
text |
Street suffic in the customer's address (e.g., Lane, Drive). |
|
SubName |
text |
Name of the subdivision. |
|
Township |
text |
Township in which the customer resides. |
|
WorkFlowStatus |
long integer |
Status of the work occurring at the customer's address. |
|
WorkFunction |
long integer |
The work function associated with the features (e.g., install, remove). |
|
WorkLocationID |
text |
Unique identifier for the work location associated with the customer's address. |
|
WorkRequestID |
text |
Unique identifier for the work request associated with the customer's address. |
|
ZipCode |
text |
Customer's zip code. |