Generator
Generator is an alternative, third party power source feeding into the electrical network.
Associations: None
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
ConnectionConfiguration |
text |
Code indicating type of connection of Generator; domain values include Delta and Wye. |
|
GroundReactance |
long integer |
Reactance of ground in ohms. |
|
GroundResistance |
long integer |
Resistance of ground in ohms. |
|
kW |
long integer |
Power rating in kW. |
|
MaxReactiveGeneration |
long integer |
Maximum reactive generation. |
|
NominalVoltage |
long integer |
Code indicating system voltage for which device is rated; domain values include 4.16 kV Grounded Y, 7.2 kV Grounded Y, etc. |
|
PositiveSequenceReactance |
double |
Equivalent positive sequence reactance seen at source by downstream circuit in ohms. |
|
PositiveSequenceResistance |
double |
Equivalent positive sequence resistance seen at source by downstream circuit in ohms. |
|
PowerFactor |
double |
Power factor rating, expressed as percentage. |
|
Rated KVA |
long integer |
Rated kVA. |
|
SubtransientReactance |
double |
Subtransient reactance. |
|
TransientReactance |
double |
Transient reactance. |
|
ZeroSequenceReactance |
double |
Equivalent zero sequence reactance seen at source by downstream circuit in ohms. |
|
ZeroSequenceResistance |
double |
Equivalent zero sequence resistance seen at source by downstream circuit in ohms. |