ControllableFitting
Controllable fittings can be mechanically set to control the flow of gas through pipes.
The CONTROLFITTING model name, although not required, can be used in gas traces to find all connected equipment belonging to a specific cathodic protection (CP) zone or structure through which current flows to help prevent pipe corrosion.
ControllableFitting inherits properties from the GasFitting abstract class.
Subtypes: Short Stop, Three Way Tee
Associations: None
Model Names: CONTROLFITTING
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
EmerIsolationSysStatus |
text |
Indicates whether feature defines a boundary of EmergencyIsolationSystem. Gas Tracing uses the EMERISOLATIONSYSSTATUS model name on this field. |
|
GasPressureSystemStatus |
text |
Indicates whether feature defines a boundary of GasPressureSystem. Gas Tracing uses the GASPRESSURESYSTEMSTATUS model name on this field. |
|
GasSystemStatus |
text |
Indicates whether feature defines a boundary of GasSystem. Gas Tracing uses the GASSYSTEMSTATUS model name on this field. |
|
NormalPosition |
long integer |
Normal position of Controllable Fitting; domain values include Open and Closed. Gas Tracing uses the NORMALPOSITION model name on this field. |
|
PresentPosition |
long integer |
Current position of Controllable Fitting; domain values include Open and Closed. |