GasPipe
GasPipe is an abstract class. GasPipe is represented as a complex edge feature because multiple connections are made along its length. Because gas pipe is inspected regularly, GasPipe is associated with objects capturing related information that does not require a location on the network such as LeakReport.
Features including, Distribution Main, Service, Gathering FieldPipe, Transmission Main, and Subtransmission Main derive attributes from GasPipe.
Subtypes: None
Associations: CPSystem, Crossing Inspection, Drip, Electric Survey GasPipeCasing, LeakReport, PipeExposure
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
ActualInternalDiameter |
double |
The diameter of the pipe in inches. The valid domain values for pipe size depend on the material of which the pipe is made: bare steel, cast iron, coated steel, copper, or plastic. |
|
BondedIndicator |
text |
Indicates whether GasValve is bonded; domain values are Yes and No. |
|
CoatingType |
text |
Code indicating coating used to protect GasPipe; domain values include Asphalt, CoalTar, and Epoxy. |
|
Comments |
text |
User or designer comments. |
|
CPSystemObjectID |
long integer |
ObjectID of associated Cathodic Protection System. |
|
CPSystemStatus |
text |
Status of associated Cathodic Protection System. |
|
DesignPressureEntered |
double |
System pressure, in any unit of measure. |
|
DesignPressureStandard |
double |
Derived field displaying calculated standard system pressure. |
|
DesignPressureUnitOfMeasure |
text |
System pressure standard unit of measure. |
|
ElectricSurveyIndicator |
text |
Code indicating whether electric survey is performed; domain values are Yes and No. |
|
EmerIsolationSysObjectID |
long integer |
ObjectID of associated Emergency Isolation System. |
|
Enabled |
text |
Users can prevent features from participating in trace results by changing the value of the Enabled field to False. |
|
GasPressureSystemObjectID |
long integer |
ObjectID of associated Gas Pressure System. |
|
GasSystemObjectID |
long integer |
Utility-defined identifier of work order. |
|
GasTraceWeight |
long integer |
Information used for tracing analysis; stored in a bitgate. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
InServiceDate |
date |
Date pipe set in service. |
|
InstallationDate |
date |
Date of installation. |
|
InstallationMethod |
text |
Method used to install pipe. |
|
LastLeakSurvey |
date |
Date last leak survey was performed. |
|
LeakSurveyFrequency |
text |
Frequency of leak surveys. |
|
LengthSource |
text |
Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived. |
|
Manufacturer |
text |
Code indicating name of GasPipe manufacturer; domain values include Thrall Distribution, UPONOR, Other, Unknown, etc. |
|
MeasuredLength |
double |
Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived. |
|
NominalDiameter |
text |
The nominal diameter identifies the size of a steel pipe without compromising the actual diameter data; domain values include 3/8”, 6”, 20”, 36”, etc. |
|
NominalDiameterUnits |
text |
Nominal Diameter standard unit of measure. |
|
OperatingPressure |
double |
The operating pressure of the pipe. |
|
Owner |
text |
Owner of GasPipe. |
|
PipeStatusIndicator |
long integer |
Code indicating status of GasPipe; domain values include Open and Closed. |
|
PipeTestDate |
date |
Date late pipe test was performed. |
|
PipeTestDuration |
text |
Duration of last pipe test. |
|
PipeTestPressure |
text |
Pressure during last pipe test. |
|
PipeTestType |
text |
Code indicating type of pipe test; domain values include Air, Gas, and Water. |
|
PipeType |
text |
Code indicating type of pipe; domain values include Non- Pinchable and Pinchable. |
|
PlasticType |
text |
Code indicating type of plastic used in GasPipe; domain values include Polyethylene and PVC. |
|
PropertyUnitCode |
text |
Value assigned to assets to track and classify Property Records. |
|
SOPEntered |
double |
System operating pressure, in any unit of measure. |
|
SOPRange |
text |
Range of system operating pressure. |
|
SOPStandard |
double |
Derived field displaying calculated standard system operating pressure. |
|
SOPUnitOfMeasure |
text |
Standard unit of measure for System Operating Pressure; examples include psi, iwc, etc. |
|
WallThickness |
text |
Thickness of pipe wall. |
|
WorkOrderID |
text |
Utility-defined identifier of work order. |