Riser
A Riser is a cylindrical or channel enclosure attached to a pole or structure to provide protection for underground conduit as it transitions from overhead to underground. The physical connection between the overhead and underground connection occurs at a pothead.

The Riser class inherits attributes from the Structure abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
ConstructionType |
text |
Code indicating construction type of Riser; domain values include 1 Phase Pothead, 3 Phase Riser with Fiberglass Arms, etc. |
|
Height |
text |
Mounting height of riser on SupportStructure. |
|
Material |
text |
Code indicating material of riser; domain values include Fiberglass, PVC, etc. |
|
SymbolRotation |
double |
Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features. |