RuralTap
Taps are used to provide service connections on gas pipes and mains. Rural Tap represents supply from transmission pipe.
RuralTap inherits characteristics from the abstract class GasDevice.
Subtypes: None
Associations: Meter, Regulator, Odorizer
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
InstallationDate |
date |
Date of installation. |
|
Manufacturer |
text |
Code indicating manufacturer. |
|
Model |
text |
RuralTap model number specified by manufacturer. |
|
OdorizerIndicator |
text |
Code indicating presence of odorizer; domain values include Yes and No. |
|
PipeLineOperator |
text |
Code indicating pipeline operator; domain values include American Natural Resources, Entex, etc. |
|
PipeLineStation |
text |
Pipeline station associated with StationStructure. |
|
ShutOffValveDiameter |
text |
Diameter of shutoff valve associated with Rural Tap; domain values include ¼”, 5/8”, 12”, 26”, etc. |
|
ShutOffValveType |
text |
Code indicating type of valve; domain values include Ball Valve, Check, Gate Valve, Wafer, etc. |
|
TapDiameter |
text |
Diameter of tap. |
|
TapType |
text |
Type of tap. |