CPTestPoint
CPTestPoint represents the test point or read point locations along a gas pipe used to test the current status of the cathodic protection system.
CPTestPoint acquires properties from the CathodicProtectionDevice abstract class.
Subtypes: None
Associations: None
Model Names: GASNONTRACABLE, TESTPOINT
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CPSystemObjectID |
long integer |
ObjectID of associated CPSystem. |
|
Name |
text |
Utility-assigned name of feature. |
|
NextTestDate |
date |
Date of next test. |
|
TestPointType |
text |
Code indicating type of CPTestPoint; domain values include Above Ground, Buried, and On Post. |
|
WireCount |
text |
Number of wires associated with test point; domain values are One Wire, Two Wires, and Unknown. |