Reclose Sequence
This object is required to enable the Network Adapter CIM export to DMS.
Associations: DynamicProtectiveDevice (only valid for subtype Recloser)
Subtypes: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Step |
short integer |
The ordinal position of the reclose step relative to other steps in the sequence. |
|
Delay |
double integer |
The time lapse before the reclose step will execute the reclose. |
|
FastType |
long integer |
True if the reclosing step is fast; otherwise, false. |