Surface Structure
SurfaceStructure contains objects that protect or enclose electric circuits and equipment on the ground. SurfaceStructure inherits attributes from the Structure abstract class.
Subtypes: Connection Box, Enclosure, Mat, Non-Electric Enclosure, Pad, Pedestal. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.
Associations: None
Model Names: STRUCTURE
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
Manufacturer |
text |
Manufacturer of support structure. |
|
Material |
text |
Code indicating material of structure; domain values include Aluminum, Fiberglass, Wood, etc. |
|
Model |
text |
Model type of SurfaceStructure. |
|
Name |
text |
Name of SurfaceStructure. |
|
StructureSize |
text |
Size of SurfaceStructure. |