Circuit Source
A circuit (feeder) is the aggregate of the conductors and equipment downstream of a substation breaker or recloser. CircuitSource stores attributes that describe characteristics of the circuit measured or estimated at the breaker or recloser. These attributes include capacity, measured in kilowatts (kW); resistance, measured in ohms; and load, measured in reactive kilovolt-amperes (kVAR).
Associations: BusBar, CircuitBreaker, Recloser
Subtypes: kW, Swing, Voltage Controlled. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.
Model Names: CIRCUITSOURCE
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
BusBarObjectID |
long integer |
ObjectID of associated BusBar. |
|
ConnectionConfiguration |
text |
Code indicating configuration of conductors; domain values include Delta, Wye, etc. |
|
DynamicProtectiveDevObjectID |
long integer |
ObjectID of associated dynamic protective device. |
|
EmergencyCapacitykW |
long integer |
Emergency rating of CircuitSource, in KW; domain values include 12. |
|
FeederSourceInfo |
long integer |
Stores information about source of feeder. Feeder Manager requires the FEEDERSOURCEINFO model name on this field. Feeder Manager uses this field to determine whether a feeder has features that participate either loop or multifeed situations. |
|
GroundReactance |
double |
Reactance of ground seen at the source by the downstream circuit. |
|
GroundResistence |
double |
Resistance of ground seen at the source by the downstream circuit. |
|
Hyperlink |
text |
Used to store a hyperlink path via standard Esri hyperlinking functionality. |
|
ID |
text |
System-generated identifier of feeder initiated at this source. Feeder Manager uses the FEEDERID model name on this field. |
|
MaximumCapacitykW |
long integer |
Maximum allowable operating capacity of CircuitSource; domain values include 10. |
|
MaxKVAR |
long integer |
Maximum kVAR load experienced at CircuitSource; domain values include 6. |
|
MaxPositiveSequenceReactance |
double |
Maximum positive sequence reactance seen at the source by the downstream circuit in ohms. |
|
MaxPositiveSequenceResistance |
double |
Maximum positive sequence resistance seen at the source by the downstream circuit in ohms. |
|
MaxZeroSequenceReactance |
double |
Maximum zero sequence reactance seen at the source by the downstream circuit in ohms. |
|
MaxZeroSequenceResistance |
double |
Maximum zero sequence resistance seen at the source by the downstream circuit in ohms. |
|
MinFaultCurrentOH |
long integer |
Calculated minimum fault current for overhead conductors. |
|
MinFaultCurrentUG |
long integer |
Calculated minimum fault current for underground conductors. |
|
MinkVAR |
long integer |
Minimum kVAR load experienced at CircuitSource; domain values include 500, etc. |
|
MinPositiveSequenceReactance |
double |
Minimum positive sequence reactance seen at the source by the downstream circuit in ohms. |
|
MinPositiveSequenceResistance |
double |
Minimum positive sequence resistance seen at the source by the downstream circuit in ohms. |
|
MinZeroSequenceReactance |
double |
Minimum zero sequence reactance seen at the source by the downstream circuit in ohms. |
|
MinZeroSequenceResistance |
double |
Minimum zero sequence resistance seen at the source by the downstream circuit in ohms. |
|
Name |
text |
Utility name of CircuitSource. Feeder Manager uses the FEEDERNAME model name on this field. |
|
NominalVoltage |
long integer |
Code indicating system voltage for which CircuitSource is rated; domain values include 7.2 kV Grounded Y, 24.9 kV Grounded Y, 2400 Delta, etc. |
|
OperatingVoltage |
long integer |
Code indicating standard level of voltage at which system is currently operated in kV; domain values include 12.5 kV Grounded Y, 7.2 kV Grounded Y, etc. |
|
SubstationID |
text |
Substation identifier. Feeder Manager uses the SUBSTATIONID model name on this field to identify the substation that acts as a source. |
|
VoltageAngle |
double |
Angle at which phase is offset from system standard. |