Vault
Vaults protect and provide access to underground gas pipes and valves.
Vault inherits attributes from the GasStructure abstract class.
Subtypes: None
Associations: None
Model Names: None
Attributes:
|
Field Name |
Field Type |
Description |
|---|---|---|
|
CoverDiameter |
double |
Diameter of vault cover (if round) in inches. |
|
CoverLength |
double |
Length of cover (if nonround) in inches. |
|
CoverWidth |
double |
Width of cover (if nonround) in inches. |
|
VentingIndicator |
text |
Code indicating whether vault is vented; domain values include Yes and No. |