DOCA0214EN–06

Remote Transfer Condition

If either source is in range, transfer will be successful. If both sources are out of range, remote transfer command will still be responded, but the result of transferring to the target source is not guaranteed.

Below is the supported voltage deviation range for RTSE with different rated voltage:

  • 380–440 V: 274 - 517 V

  • 208–240 V: 174 -280 V

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?