DOCA0214EN–06

Undervoltage Thresholds

Field

Description

Default value

  • Dropout: 85% of the rated voltage.

  • Pickup: 90% of the rated voltage.

Range

  • Range for falling voltage (dropout) is 70%-95% of the rated voltage.

  • Range for return voltage (pickup) is 85%–100% of the rated voltage.

Adjustable

The adjustable step for an undervoltage threshold is 1%.

Differential

  • The differential between dropout and pickup is equal to 2% of rated voltage.

On LCD display

  • If minimum 2% differential of rated voltage rule is broken during dropout setting, the pickup value will be modified dynamically (pickup = dropout + 2%) to keep the rule.

On Modbus

Modbus register write: The dropout value is always accepted. The pickup value will be modified to a value (pickup = dropout + 2%) when the pickup value does not comply the minimum differential.

Sequence of events

  • When a sensor detects a voltage below the dropout set voltage for a period longer than the time delay, it will deem the voltage for out of range.

  • When a sensor detects a voltage at or above the pickup point, it will deem the voltage as acceptable.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?