DOCA0214EN–06

Terminal Cover

DANGER
HAZARD OF FLASH OVER BETWEEN POLARITIES
Terminal cover must be installed after wiring to ensure proper insulation.
Failure to follow these instructions will result in death or serious injury.
WARNING
UNGUARDED MACHINERY HAZARD
Install the terminal cover correctly after wiring, to ensure the insulation distance.
Failure to follow these instructions will result in death or serious injury.

Terminal covers are used between the power terminals to provide insulation between phases. They are supported on TransferPacT Active Automatic / Automatic 32-100 A and 80-160 A transfer switching equipment only.

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic 32-100 A: JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A: JYT3049901

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?