Threshold
|
Description |
Settings |
Default
setting |
Adjustment range |
Note |
|---|---|---|---|---|
|
Voltage |
Delta Dropout (under and over voltage) |
10% |
4 -> 20% |
Step of 2% |
|
Delta Pickup |
20% of delta drop out |
fixed |
fixed |
|
|
Frequency |
Delta Dropout |
5% |
2 -> 10% |
Step of 1% |
|
Delta Pickup |
20% of delta drop out |
fixed |
fixed |
The accuracy of voltage sensing is 1%.
The accuracy of frequency sensing is 0.1%.