DOCA0214EN–06

Load Extension Bar

Load extension bars are used to connect the power terminals of switch and cables for load side.

The table below provides the list of load extension bars:

Switch

Number of poles

Load extension bar

Frame 100: 32–100 A

4P

TPSCON35

Frame 160: 80–160 A

4P

TPSCON36

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic 32-100 A: JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A: JYT3049901

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?