Time Delay
|
- |
Adjust |
Range |
Default |
||
|---|---|---|---|---|---|
|
Symbol |
Display |
Definition |
Active automatic |
Active automatic |
Active automatic |
|
T2 |
Transfer Delay |
Confirmation delay on source power failure |
0.1 s from 0-1 s. 1 s when >1 s. |
0-1800 s |
3 s |
|
T4 |
Center-off Delay |
OFF position delay |
1 s |
0-30 s |
0 s |
|
T6 |
Re-transfer Delay |
Confirmation delay to re-transfer on normal source |
1 s |
0-3600 s |
60 s |
|
T7 |
Genset Start Delay |
Delay to start Genset |
1 s |
0-120 s |
3 s |
|
T8 |
Loadshed Delay |
Delay to load shedding |
1 s |
0-15 s |
0 s |
|
T9 |
Genset cool delay |
Genset cooling down delay |
1 s |
0-3600 s |
60 s |
|
T10 |
Genset fail delay |
Genset alarming failure detection time |
1 s |
15–300 s |
300 s |
|
T13 |
On load test delay |
Time duration to run for test process on load. |
1 s |
Unlimited: 0 s Limited: 1-1800 s |
Unlimited: 0 s Limited: 30 s |
|
T14 |
Off load test delay |
Time duration to run for test process off load. |
1 s |
Unlimited: 0 s Limited: 1-1800 s |
Unlimited: 0 s Limited: 30 s |
T2: Transfer Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
3 s |
|
Range |
0–1800 s |
|
Adjust |
Step of 0.1 s from 0-1 s. 1 s when >1 s. |
T4: Center-Off Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
0 s |
|
Range |
0–30 s |
|
Adjust |
Step of 1 s |
T6: Re-Transfer Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
60 s |
|
Range |
0–3600 s |
|
Adjust |
Step of 1 s |
T7: Genset Start Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
3 s |
|
Range |
0–120 s |
|
Adjust |
Step of 1 s |
T8: Loadshed Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
0 s |
|
Range |
0–15 s |
|
Adjust |
Step of 1 s |
T9: Genset Cool Delay
|
Field |
Description |
|---|---|
|
Applications |
NOTE: To prevent any risk of Genset damage due to Genset stopping
before the end of its starting process: Genset cooling time delay
can only start after the end of Genset start time delay or after SII
is within tolerances since source return time delay.
|
|
Default values |
60 s |
|
Range |
0–3600 s |
|
Adjust |
Step of 1 s |
T10: Genset Fail Delay
|
Field |
Description |
|---|---|
|
Applications |
|
|
Default values |
|
|
Range |
15–300 s |
|
Adjust |
Step of 1 s |
T13: On Load Test Delay
|
Field |
Description |
|---|---|
|
Applications |
Time duration for On load test process. It will rise the alarm if test is not finished in the time duration. |
|
Default values |
|
|
Range |
1–1800 s |
|
Adjust |
Step of 1 s |
T14: Off Load Test Delay
|
Field |
Description |
|---|---|
|
Applications |
Time duration for off load test process. It will rise the Alarm if test is not finished in the time duration. |
|
Default values |
|
|
Range |
1–1800 s |
|
Adjust |
Step of 1 s |