Voluntary Remote Control
The voluntary remote control is an accessory module installed on TransferPacT Automatic and TransferPacT Active Automatic controller with the following functions:
-
Voluntary remote control to N or A, 2 NO contacts are provided.
-
Force to off, 1 NO contact is provided.
-
Green LED on the front face of the accessory indicates the power status and proper connection of the accessory.
-
Communication with the main MCU on ATSE.
-
Only one voluntary remote controller module is allowed to be installed on the product.
Application Voluntary to N or A
Voluntary transfer is an active input which can transfer the ATSE to normal or alternate source according to requirements (such as energy saving).
Voluntary transfer will still keep the power continuity as much as possible. The function will be bypassed, if target source lost the power. For example, after voluntary to A while A source failed, ATSE will transfer back to N if N is available.
Exit the voluntary mode after signal disappeared.
Force to Off
Force to Off is an emergency stop order, to transfer the ATSE to off position. All the other transfer mode will be canceled except handle control.
Exit Force to Off after signal disappeared.
Terminals
There are three terminals of the voluntary remote controller modules as below:
-
V1-V0: voluntary to N
-
V2-V0: voluntary to A
-
F1-V0: force to Off
Signal Type
-
Digital input with dry contact.
-
Need over 200 ms input to start voluntary remote control.
Performance
|
Electrical characteristics |
Ratings |
|---|---|
|
Ui |
30 VDC |
|
Minimum input current |
5 mA |
|
Altitude |
2000 m |
Cable Capacity for Terminals
The cable capacity for the terminals are 0.05 – 2.6 mm2 (AWG 30 ~ 13).