DOCA0214EN–04

Voltage Dropout and Pickup


  • Over voltage dropout value: Above this value, the voltage is out of range and transfer is initiated.

  • Over voltage pickup value: When voltage goes back from over frequency, it is a condition to go back to normal situation.

  • Under voltage dropout value: Below this value, the frequency is out of range and transfer is initiated.

  • Under voltage pickup value: When voltage goes back from under voltage, it is a condition to go back to normal situation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?