DOCA0214EN–06

Status Page

  1. Select Status and press OK button to open its sub-pages.

  2. Press Up and Down buttons to navigate to each sub-page.

The below table provide the details of the Status sub-pages:

Sub-page name

Sub-page function

Display

Slots

Slots Status sub-page navigates to more status checking in the display and click Slots to check status of accessories slots.

To show the Slot status:

  • Black box indicates that the accessories has inserted well.

  • Empty box indicates that the accessories has not inserted or not inserted well.

Transfer Diagnostic

Transfer Diag sub-page navigates to more status checking in the display and click Transfer Diag to check the transfer times.

Transfer Diag sub-page is to show the transfer times:

  • Successful transfer counts

  • Failed transfer counts

  • Too many transfer counts

Event Logs

Event Logs Status sub-page navigates to more status checking in the display and click Event Logs to check list of logs.

Event Logs sub-page is to show the list of event logs:

  • Use up and down button for navigation.

  • Click Event Log XX to check status of logs.

Event Logs

Event Logs sub-page is to show the information of event logs:

  • Time of events.

  • Source status during events.

For more information on Event Code, refer to Event Logs.

Detailed Info

To show the cause of events:

  • Transfer mode during events.

  • Type of events.

Version

Version Status sub-page navigates to more status checking in the display and click Version to check product information.

To show the list of hardware components:

  • Use up and down button for navigation.

  • Click different components to check their information.

Controller

To show the components information

  • Series number of components.

  • Firmware version.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?