Warning
When the warning is triggered for event codes, such as 30,31,40,41,50,51,52 and 53, the HMI will pop-up the alarm screen. The green source LED blinks OFF or ON for event codes such as 54,55,70,71,72,73,74,75,76,77,78,79,80 and 81. The event code list and display method are shown in the below table.
The icon is displayed on the page
to indicate an active warning.
If the warning is triggered, it will display the latest warning and previous alarms are overwritten on the HMI. The log will be recorded.
Perform the following procedure to check and clear the alarm:
-
Select the Set & Operate page and press OK.
-
Enter the password to open the Set & Operate page.
-
Select Operations sub-page.
-
Press Down button and select Warning Ack.
-
Click OK on the screen.
The warning will not inhibit the transfer functions for the below event codes:
List of Event Codes
|
Alarm code |
Alarm message |
LCD display method |
LED display method |
|---|---|---|---|
|
30 |
Genset invalid |
Bottom bar |
None |
|
31 |
Genset start failure |
Bottom bar |
None |
|
40 |
On load test failure |
Bottom bar |
None |
|
41 |
Off load test failure |
Bottom bar |
None |
|
42 |
On load test success |
Bottom bar |
None |
|
43 |
Off load test success |
Bottom bar |
None |
|
50 |
SI unbalance warning |
Bottom bar |
None |
|
51 |
SII unbalance warning |
Bottom bar |
None |
|
52 |
SI neutral position wrong warning |
Bottom bar |
None |
|
53 |
SII neutral position wrong warning |
Bottom bar |
None |
|
54 |
SI neutral loss warning |
None |
LED source state blinking |
|
55 |
SII neutral loss warning |
None |
LED source state blinking |
|
70 |
SI under voltage |
None |
LED source state blinking |
|
71 |
SII under voltage |
None |
LED source state blinking |
|
72 |
SI over voltage |
None |
LED source state blinking |
|
73 |
SII over voltage |
None |
LED source state blinking |
|
74 |
SI no voltage |
None |
LED source state off |
|
75 |
SII no voltage |
None |
LED source state off |
|
76 |
SI under frequency |
None |
LED source state blinking |
|
77 |
SII under frequency |
None |
LED source state blinking |
|
78 |
SI over frequency |
None |
LED source state blinking |
|
79 |
SII over frequency |
None |
LED source state blinking |
|
80 |
SI all recover |
None |
LED source state on |
|
81 |
SII all recover |
None |
LED source state on |
SI Unbalance Warning
-
Event code: 50.
-
Type of event: Warning.
-
Default: Disable.
-
Description: If unbalance of voltage occurs over the drop-out rate of threshold (5% as default) when SI is connected, a warning will be raised.
-
Cause: Too many single-phase loads or poor quality of power supply environment.
-
Diagnosis and repair: Set the different value of imbalance rate or contact field service.
SII Unbalance Warning
-
Event code: 51.
-
Type of event: Warning.
-
Default: Disable.
-
Description: If unbalance of voltage occurs over the drop-out rate of threshold (5% as default) when SII is connected, a warning will be raised.
-
Cause: Too many single-phase loads or poor quality of power supply environment.
-
Diagnosis and repair: Set the different value of imbalance rate or contact field service.
Generator Invalid
-
Event code: 30.
-
Type of event: Warning.
-
Default: Always disable.
-
Description: The sudden loss of an alternate source will lead to a warning.
-
Cause: Genset is not connected well or some failure on Genset started
-
Diagnosis and repair: Contact field service.
Generator Start Failure
-
Event code: 31.
-
Type of event: Warning.
-
Default: Disable.
-
Description: After sending the Genset start signal, controller will wait a time T10 duration until Genset is ready.
-
The ATSE will rise the Genset alarm, if Genset is not started within T10 timer is ended (if enabled).
-
The ATSE shall reset the Genset alarm, when the A source is in range or when the N source is in range.
-
The time delay is only available when there is external power.
-
-
Cause: Genset is not connected well or some failure on Genset started.
-
Diagnosis and repair: Contact field service.
On Load/Off Load Test Failure
-
Event code: 40, 41
-
Type of event: Warning.
-
Default: Always enabled.
-
Description: If on load or off load test is failed or interrupted, a warning will be raised.
-
Cause: Product failure or external interruption
-
Diagnosis and repair: Contact field service.
SI or SII Neutral Position Wrong Warning
-
Event code: 52, 53
-
Type of event: Warning.
-
Default: Always enabled in IEC market, disabled in China market.
-
Description: If sequence of neutral is not connected as set value, a warning will be raised.
-
Cause: Wrong connection of neutral or wrong settings.
-
Diagnosis and repair: Set the new neutral sequence or contact field service.
SI or SII Neutral Loss Warning
-
Event code: 54, 55
-
Type of event: Warning.
-
Default: Disabled.
-
Description: If unbalance rate of voltage occurs over 20% when source is connected, a warning will be raised.
-
Cause: Miss connection or disconnection caused by interior or exterior impacts of neutral line..
-
Diagnosis and repair: correct the connection or contact field service.
SI Under Voltage
-
Event code: 70.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When there is under voltage on SI, an event log will be recorded.
SII Under Voltage
-
Event code: 71.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When there is under voltage on SII, an event log will be recorded.
SI Over Voltage
-
Event code: 72.
-
Type of event: Event.
-
Default: Disabled.
-
Description: When there is over voltage on SI, an event log will be recorded.
SII Over Voltage
-
Event code: 73.
-
Type of event: Event.
-
Default: Disabled.
-
Description: When there is over voltage on SII, an event log will be recorded.
SI No Voltage
-
Event code: 74.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When there is source failure on SI, an event log will be recorded.
SII No Voltage
-
Event code: 75.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When there is source failure on SII, an event log will be recorded.
SI Under Frequency
-
Event code: 76.
-
Type of event: Event.
-
Default: Disable
-
Description: When there is Under frequency on SI, an event log will be recorded.
SII Under Frequency
-
Event code: 77.
-
Type of event: Event.
-
Default: Disable
-
Description: When there is Under frequency on SII, an event log will be recorded.
SI Over Frequency
-
Event code: 78.
-
Type of event: Event.
-
Default: Disable
-
Description: When there is Under frequency on SI, an event log will be recorded.
SII Over Frequency
-
Event code: 79.
-
Type of event: Event.
-
Default: Disable
-
Description: When there is Under frequency on SII, an event log will be recorded.
SI All Recover
-
Event code: 80.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When SI recover to normal, an event log will be recorded.
SII All Recover
-
Event code: 81.
-
Type of event: Event.
-
Default: Always enable.
-
Description: When SII recover to normal, an event log will be recorded.