DOCA0214EN–06

Alarm

When an alarm is triggered, it will ignore all other alarms and the alarm LED shall always be ON until it is acknowledged.

NOTE: The Modbus will provide the other alarms continuously.

The following are the methods to clear/acknowledge alarms:

  • For TransferPacT Remote, cancel the alarm by resetting RTSE at site.

  • For Automatic HMI, put the dielectric switch to TEST position and then put it back to RUN to restart the controller to clear/acknowledged the alarm.

  • For Active Automatic HMI, when an alarm is triggered, the HMI will pop-up alarm screen. There will be a icon displayed on the page to indicate that there is an active alarm.

Perform the following procedure to check and clear the alarm on Active Automatic:

  1. Select the Set & Operate page and press OK.

  2. Enter the password to open the Set & Operate page.

  3. Select Operations sub-page.

  4. Press Down button and select Alarm Ack.

  5. Click OK on the screen.

NOTE: A password is required to open the Set & Operate page.

Alarm Message

Alarm Code

Alarm Message

LCD display

1

Position alarm: transfer to A error

Transfer to A failed

2

Position alarm: transfer to N error

Transfer to N failed

3

Position alarm: transfer to OFF error

Transfer to OFF failed

4

Position alarm: transfer to invalid position

Invalid position

5

Position Alarm: Internal error

Internal error

6

Position alarm: unexpected position

Unexpected position

10

Source I phase rotation error

SI phase rotation

11

Source II phase rotation error

SII phase rotation

12

Unsupported device RS alarm

Unsupported device RS

Position Alarm: Transfer to A Error

  • Event code: 1

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When TSE cannot transfer to replacement, an alarm will be raised.

  • Cause: Stack of mechanism or failure of electronic components.

  • Diagnosis and repair: Contact field service.

Position Alarm: Transfer to N Error

  • Event code: 2.

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When the TSE cannot transfer to normal, an alarm will be raised.

  • Cause: Stack of mechanism or failure of electronic components.

  • Diagnosis and repair: Contact field service.

Position Alarm: Transfer to Off Error

  • Event code: 3.

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When the TSE cannot transfer to off position, an alarm will be raised.

  • Cause: Stack of mechanism or failure of electronic components.

  • Diagnosis and repair: Contact field service.

    .

Position Alarm: Transfer to Invalid Position

  • Event code: 4.

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When TSE transfer to frequently, an alarm will be raised.

  • Cause: Unexpected operating or controller failure.

  • Diagnosis and repair: Contact field service.

    .

Position Alarm: Internal Error

  • Event code: 5

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When TSE cannot transfer to off position, an alarm will be raised.

  • Cause: Stack of mechanism or failure of electronic components.

  • Diagnosis and repair: Contact field service.

    .

Position Alarm: Unexpected Position

  • Event code: 6

  • Type of event: Alarm.

  • Default: Always enable.

  • Description: When micro-switch all closed, the TSE may lead short circuit of two sources. an alarm will be raised.

  • Cause: Welding issue of failure of micro-switch.

  • Diagnosis and repair: Contact field service.

Source I or II Phase Rotation Failure

  • Event code: 10,11.

  • Type of event: Alarm.

  • Default: Enabled (Disabled in China market)

  • Description: When there is phase rotation such as from A-B-C move to C-B-A, an alarm will be raised if this function is enabled.

  • Cause: Wrong installing when first connection of main circuit or reform the main connections.

  • Diagnosis and repair: Double check the phase sequence of main circuit or contact field service.

Unsupported Device RS Alarm

  • Event code: 12.

  • Type of event: Alarm.

  • Default: Always enabled.

  • Description: If a rotary switch is connected to a frame 250, 630 or 800 TSE with operation voltage from 208-250 V, an alarm will be raised.

  • Cause: Rotary switch is not supported on the frame 250, 630 or 800 TSE with operation voltage from 208-250 V.

  • Diagnosis and repair: Remove the rotary switch if it's connected or contact field service.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?