DOCA0214EN–06

Settings Sub-Page

The below table provide the details of the Settings sub-pages:

Sub-page name

Sub-page function

Display

Settings

Set & Operate page navigates to more set & operate option in the display.

Click Settings for accessories commissioning, reset and password settings.

Accessories

Accessories is a sub-page of Settings.

Accessories page navigates to more setting option in the display.

Modbus

Modbus is a sub-page of Accessories.

Click Modbus for commissioning.

NOTE: If the module of Modbus is not inserted, the option will be empty.

Select the parameters as below:

  • Set the Address

  • Set the Baudrate

NOTE: The odd/even parity is automatically recognized.

Confirm Operation

Confirm Operation window is to confirm the Modbus and click OK to save changes.

DI Test

DI Test is a sub-page of Accessories.

Click DI Test for commissioning.

NOTE: If the module of remote test is not inserted, the option will be empty.

Set On Load Test or Off Load Test.

Confirm Operation

Confirm Operation window is to confirm the DI Test and click OK to save changes.

Quick View Auto Scroll

Quick View Auto Scroll is a sub-page of Settings.

Quick View Auto Scroll page navigates to more settings option in the display.

NOTE: If the module of Quick View Auto Scroll test is not inserted, the option will be empty.

Select Quick View Auto Scroll to set the conditions:

  • ON: enable Quick View Auto Scroll detection.

  • OFF: disable Quick View Auto Scroll detection.

NOTE: Default setting is shown as disabled.

Select Scroll Time and use up or down button to set it. The range of quick view auto scroll time is from 0 ~300 s with step of 1 s.

Default value is 5 s.

Change Password

Change Password is a sub-page of Settings.

Click Change Password to change password.

Select the parameters to change password:

  • Input 4 digital code to create new password.

NOTE: To change or reset the password:
  1. Change to handle mode.

  2. Restart the ATSE.

  3. Press OK and ESC button for 10 seconds.

NOTE: The step 3 should be performed within 1 minute after step 2.

System Logs

System Logs is a sub-page of Settings.

Select System Logs and use up or down button to set it.

Reset Threshold & tim.

Reset Threshold & tim. is a sub-page of Settings.

Click Reset Threshold & tim. to reset the controller.

List of values that can be reset:

  • Under Voltage

  • Over Voltage

  • Under Frequency

  • Over Frequency

  • Unbalance Rate

  • Transfer Delay (T2)

  • Center-Off Delay (T4)

  • Re-Transfer Delay (T6)

  • Genset Start Delay (T7)

  • Loadshed Delay (T8)

  • Genset Cool Delay (T9)

  • Genset Fail Delay (T10)

  • On Load Test Delay (T13)

  • Off Load Test Delay (T14)

Confirm Operation

Confirm Operation window is to confirm the Reset Threshold & tim. and click OK to save changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?