DOCA0214EN–06

Operations Sub-Page

NOTE: Once the TransferPacT ATSE is power ON for the first time, suggested to change the password. The default password is 0000.

The below table provide the details of the Operations sub-pages:

Sub-page name

Sub-page function

Display

Operations

Set & Operate page navigates to more maintenance checking in the display and click Operations to control the ATSE or acknowledge the alarm.

Warning Acknowledge

Click Warning Ack to cancel the alarm.

Confirm Operation

Confirm Operation window is to confirm the Warning Acknowledge.

Alarm Acknowledge

Click Alarm Ack to cancel the alarm.

Confirm Operation

Confirm Operation window is to confirm the Alarm Acknowledge.

Local Control

Click Local Control to enter local control mode.

  • When open the first page, the local control is disabled.

  • Click Enable Local Control to energize local control mode.

  • Local Control cannot be enabled under handle mode, force mode, and fire protection mode.

Confirm Operation

Confirm Operation window is to confirm the Local Control.

Disable Local Control

Disable Local Control is a sub-page of Local Control.

Select the Disable Local Control again to exit local control mode.

NOTE: If exit this page without disable local control mode, the transfer switch will stay at local control mode until a control mode with higher priority is coming

at the bottom indicates the transfer mode.

Confirm Operation

Confirm Operation window is to confirm the Local Control.

Transfer to SI(N)

Transfer to SII(A)

Transfer to OFF

Transfer to SI(N) and Transfer to SII(A) depends on target source status, Transfer to OFF always active.

After enabling the Local Control, there are three options:

  • Click Transfer to SI (N) to transfer the switch to normal.

  • Click Transfer to SII (A) to transfer the switch to alternative.

  • Click Transfer to OFF to transfer the switch to OFF.

NOTE: Transfer to N or A will be successful only when the target source is present and in range.

Confirm Operation

Confirm Operation window is to confirm the Local Control.

Comm Control

Click Comm Control to enter communication control mode.

Comm control navigates to more COM operation in the display.

Transfer by Comm

Transfer by Comm is a sub-page of Comm Control.

Select Transfer by Comm to set the operation:

  • ON: enable transfer by com function.

  • OFF: disable transfer by com function.

NOTE: The function is disabled by default.

Confirm Operation

Confirm Operation window is to confirm the Transfer by Comm and click OK to save changes.

Test by Comm

Test by Comm is a sub-page of Comm Control.

Select Tesy by Comm to set the operation:

  • ON: enable test by com function.

  • OFF: disable test by com function.

NOTE: The function is disabled by default.

Confirm Operation

Confirm Operation window is to confirm the Test by Comm and click OK to save changes.

On Load Test

Operations sub-page navigates to more operating option in the display and click On Load Test to enter test mode.

Confirm Operation

Confirm Operation window is to confirm the On Load Test.

Test in Progress

The icon indicates that the test is started. Test can be interrupted during the process.

NOTE: Select ESC and click OK to stop the test, ATSE will go back to Auto mode.

Confirm Operation

Confirm Operation window is to confirm the On Load Test.

Off Load Test

Click Off Load Test to enter test mode.

 

Confirm Operation

Confirm Operation window is to confirm the Off Load Test.

Confirm to select Limited test or Unlimited test

limited test

unlimited test

Test in Progress

The icon indicates that the test is started. Test can be interrupted during the process.

NOTE:

Select ESC and click OKto stop the test, ATSE will go back to Auto mode.

limited test

unlimited test

Confirm Operation

Confirm Operation window is to confirm the Off Load Test.

unlimited test

 
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?