DOCA0214EN–06

Frequency Dropout and Pickup


  • Over frequency dropout value: Above this value, the frequency is out of range and transfer is initiated.

  • Over frequency pickup value: When frequency goes back from over frequency, it is a condition to go back to normal situation.

  • Under frequency dropout value: Below this value, the frequency is out of range and transfer is initiated.

  • Under frequency pickup value: When frequency goes back from under frequency, it is a condition to go back to normal situation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?