DOCA0214EN–06

Aluminum Connector

DANGER
Hazard of electric shock, explosion or arc flash
It is mandatory to install terminal shield when the connectors are used.
Failure to follow these instructions will result in death or serious injury.

Aluminum connectors can be used to connect the switch and power cables. It supports to connect up to six cables simultaneously.

Aluminum connectors are screwed on the switch using the screws delivered with the aluminum connectors.

The table below provides the list of aluminum connectors.

Switch

Number of poles

Aluminum connector

Number of cables

Frame 250: 100–250 A

3P

LV429227

1

LV429259

1

TPSCON49 (1)

1

TPSCON51

2

TPSCON47

6

4P

LV429228

1

LV429260

1

TPSCON50

1

TPSCON52 (1)

2

TPSCON48

6

Frame 630: 320–630 A

3P

TPSCON53

1

4P

TPSCON54

1

Frame 1600: 800–1250 A

3P

33640

4

4P

33641

4

(1) Aluminum connectors for load terminals only.

The bare cable connector (commercial references: 33640 and 33641) is not compatible with the spreader, vertical connection adapter or cable-lug adapter on TransferPacT Active Automatic 800–1250 A transfer switching equipment.

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic 800–1600 A: BQT7680301

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?