DOCA0214EN–06

Fire Protection Mode

  • An emergency stop order to transfer ATSE to off position. All the other transfer mode will be canceled except force to OFF and handle control. There shall be no time delay.

  • Exit fire protection after signal disappeared.

  • Require accessories TPCDIO10 or TPCDIO11 or TPCDIO13 or TPCDIO14 to extend this function.

Application

  • The fire protection signal can transfer ATSE to off position when there is fire emergency.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?