DOCA0214EN–06

Overview

There are two types of alarms for ATSE and RSTE:

  • Alarm

  • Warning

Alarm Type

Description

Alarm

Indicates the controller detects a critical error or switch mechanism error. Do not perform manual operation when ATSE is in alarm state. Contact field service first, and/or check the root cause according to the Alarm Message to clear and acknowledge the alarm.

Warning

Indicates the occurrence of unsuccessful testing, Genset start or detected failure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?