DOCA0214EN–06

Overview

TransferPacT ATSE has two embedded HMIs and one external HMI. The two embedded HMIs can be inserted on the slots of the embedded HMI. They are as below:

  • Automatic HMI with rotary switch

  • Active Automatic HMI with LCD display

The two embedded HMIs can be replaced with each other with hot swap approach.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?