DOCA0214EN–06

Wiring of Auxiliary Contacts

For information on installation of auxiliary contacts, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic 32-100 A: JYT3049801

  • TransferPacT Active Automatic / Automatic 80-160 A: JYT3049901

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

  • TransferPacT Active Automatic 800–1600 A: BQT7680301

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?