DOCA0214EN–06

Single Line Diagram Description

TransferPacT Active Automatic / Automatic 32-100, 80-160 A

TransferPacT Active Automatic / Automatic 100–250, 320–630, 800 A TransferPacT Active Automatic 800–1600 A

TransferPacT Remote 160-250, 320-630, 800 A

Label

Description

A

Source I power status indicator

B

Contact position of source I

C

Contact position of source II

D

Source II power status indicator

E

Alarm indicator

F

Not in Auto status indicator

G

Power ON indicator

H

Run status indicator

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?