Modbus Registers
The main information needed for remote supervision of a TransferPacT Switching Equipment is contained in the table of common registers starting at register 1001.
One Modbus read request is limited to 125 registers maximum. Three Modbus read requests are necessary to read the entire table.
Use of these common registers is highly recommended to optimize response times and simplify the use of data.
Table Format
Register tables have the following columns:
|
Address |
Register |
Pole number |
R/W |
Unit |
Type |
Range |
TA |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
-
Address: a 16-bit register address in hexadecimal. The address is the data used in the Modbus frame.
-
Register: a 16-bit register number in decimal (register = address + 1).
-
Pole number: number of poles that are applicable for that register.
-
R/W: register read-write status
-
R: the register can be read by using Modbus functions
-
W: the register can be written by using Modbus functions
-
RW: the register can be read and written by using Modbus functions
-
RC: the register can be read by using the command interface
-
WC: the register can be written by using the command interface
-
-
Unit: the unit the information is expressed in.
-
Type: the encoding data type (see data type description below).
-
Range: the permitted values for this variable, usually a subset of what the format allows.
-
TA: type of TransferPacT switch for which the register is available.
-
Bit: bit position applicable for that register.
-
Description: provides information about the register and restrictions that apply.
TransferPacT Switching Equipment Register
|
Address |
Register |
Pole number |
R/W |
Unit |
Type |
Range |
TA |
Bit |
Description |
||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x03E8 |
1001 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Switch position
|
||||||||||||||||||||
|
0x03EA |
1003 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Normal source state
|
||||||||||||||||||||
|
0x03EC |
1005 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Alternate source state
|
||||||||||||||||||||
|
0x03ED |
1006 |
4P |
R |
– |
BOOL |
– |
TA |
0 |
SI phase sequence error validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
4P |
R |
– |
BOOL |
– |
TA |
1 |
SI neutral position wrong validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
3P/4P |
R |
– |
BOOL |
– |
TA |
2 |
SI unbalance voltage validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
4P |
R |
– |
BOOL |
– |
TA |
3 |
SI neutral loss alarm validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
ALL |
R |
– |
BOOL |
– |
TA |
4 |
SI over voltage state validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
ALL |
R |
– |
BOOL |
– |
TA |
5 |
SI under voltage state validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
ALL |
R |
– |
BOOL |
– |
TA |
6 |
SI over frequency state validity
|
||||||||||||||||||||
|
0x03ED |
1006 |
ALL |
R |
– |
BOOL |
– |
TA |
7 |
SI under frequency state validity
|
||||||||||||||||||||
|
0x03EE |
1007 |
4P |
R |
– |
BOOL |
– |
TA |
0 |
SI phase sequence error
|
||||||||||||||||||||
|
0x03EE |
1007 |
4P |
R |
– |
BOOL |
– |
TA |
1 |
SI neutral position wrong
|
||||||||||||||||||||
|
0x03EE |
1007 |
3P/4P |
R |
– |
BOOL |
– |
TA |
2 |
SI unbalance voltage status
|
||||||||||||||||||||
|
0x03EE |
1007 |
4P |
R |
– |
BOOL |
– |
TA |
3 |
SI neutral loss alarm
|
||||||||||||||||||||
|
0x03EE |
1007 |
ALL |
R |
– |
BOOL |
– |
TA |
4 |
SI over voltage state
|
||||||||||||||||||||
|
0x03EE |
1007 |
ALL |
R |
– |
BOOL |
– |
TA |
5 |
SI under voltage state
|
||||||||||||||||||||
|
0x03EE |
1007 |
ALL |
R |
– |
BOOL |
– |
TA |
6 |
SI over frequency state
|
||||||||||||||||||||
|
0x03EE |
1007 |
ALL |
R |
– |
BOOL |
– |
TA |
7 |
SI under frequency state
|
||||||||||||||||||||
|
0x03EF |
1008 |
4P |
R |
– |
BOOL |
– |
TA |
0 |
SII phase sequence error validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
4P |
R |
– |
BOOL |
– |
TA |
1 |
SII neutral position wrong validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
3P/4P |
R |
– |
BOOL |
– |
TA |
2 |
SII unbalance voltage validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
4P |
R |
– |
BOOL |
– |
TA |
3 |
SII neutral loss alarm validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
ALL |
R |
– |
BOOL |
– |
TA |
4 |
SII over voltage state validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
ALL |
R |
– |
BOOL |
– |
TA |
5 |
SII under voltage state validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
ALL |
R |
– |
BOOL |
– |
TA |
6 |
SII over frequency state validity
|
||||||||||||||||||||
|
0x03EF |
1008 |
ALL |
R |
– |
BOOL |
– |
TA |
7 |
SII under frequency state validity
|
||||||||||||||||||||
|
0x03F0 |
1009 |
4P |
R |
– |
BOOL |
– |
TA |
0 |
SII phase sequence error
|
||||||||||||||||||||
|
0x03F0 |
1009 |
4P |
R |
– |
BOOL |
– |
TA |
1 |
SII neutral position wrong
|
||||||||||||||||||||
|
0x03F0 |
1009 |
3P/4P |
R |
– |
BOOL |
– |
TA |
2 |
SII unbalance voltage status
|
||||||||||||||||||||
|
0x03F0 |
1009 |
4P |
R |
– |
BOOL |
– |
TA |
3 |
SII neutral loss alarm
|
||||||||||||||||||||
|
0x03F0 |
1009 |
ALL |
R |
– |
BOOL |
– |
TA |
4 |
SII over voltage state
|
||||||||||||||||||||
|
0x03F0 |
1009 |
ALL |
R |
– |
BOOL |
– |
TA |
5 |
SII under voltage state
|
||||||||||||||||||||
|
0x03F0 |
1009 |
ALL |
R |
– |
BOOL |
– |
TA |
6 |
SII over frequency state
|
||||||||||||||||||||
|
0x03F0 |
1009 |
ALL |
R |
– |
BOOL |
– |
TA |
7 |
SII under frequency state
|
||||||||||||||||||||
|
0x03FC |
1021 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Load shedding function supported
|
||||||||||||||||||||
|
0x03FD |
1022 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Load shedding status
|
||||||||||||||||||||
|
0x03FE |
1023 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Genset control status supported
|
||||||||||||||||||||
|
0x03FF |
1024 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Genset control status
|
||||||||||||||||||||
|
0x044B |
1100 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Runtime mode
|
||||||||||||||||||||
|
0x044F |
1104 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Generator Ready Alarm Delay T10
|
||||||||||||||||||||
|
0x07CF |
2000 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VAB
|
||||||||||||||||||||
|
0x07D1 |
2002 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VBC
|
||||||||||||||||||||
|
0x07D3 |
2004 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VCA
|
||||||||||||||||||||
|
0x07D5 |
2006 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SI frequency
|
||||||||||||||||||||
|
0x07D7 |
2008 |
2P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VAN
|
||||||||||||||||||||
|
0x07D9 |
2010 |
4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VBN
|
||||||||||||||||||||
|
0x07DB |
2012 |
4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SI VCN
|
||||||||||||||||||||
|
0x07DD |
2014 |
3P/4P |
R |
% |
FLOAT32 |
– |
TA |
– |
SI voltage unbalance rate
|
||||||||||||||||||||
|
0x0833 |
2100 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VAB
|
||||||||||||||||||||
|
0x0835 |
2102 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VBC
|
||||||||||||||||||||
|
0x0837 |
2104 |
3P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VCA
|
||||||||||||||||||||
|
0x0839 |
2106 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SII frequency
|
||||||||||||||||||||
|
0x083B |
2108 |
2P/4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VAN
|
||||||||||||||||||||
|
0x083D |
2110 |
4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VBN
|
||||||||||||||||||||
|
0x083F |
2112 |
4P |
R |
V |
FLOAT32 |
– |
TA |
– |
SII VCN
|
||||||||||||||||||||
|
0x0841 |
2114 |
3P/4P |
R |
% |
FLOAT32 |
– |
TA |
– |
SII voltage unbalance rate
|
||||||||||||||||||||
|
0x0BB9 |
3002 |
ALL |
R/W |
V |
FLOAT32 |
– |
TA |
– |
Source rated voltage
|
||||||||||||||||||||
|
0x0BBB |
3004 |
ALL |
R/W |
Hz |
FLOAT32 |
– |
TA |
– |
Source rated frequency
|
||||||||||||||||||||
|
0x0BBD |
3006 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Source neutral position
|
||||||||||||||||||||
|
0x0BC1 |
3010 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable abnormal frequency transfer
|
||||||||||||||||||||
|
0x0BC2 |
3011 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI under frequency start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BC4 |
3013 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI under frequency reset/Pick-up threshold percent
|
||||||||||||||||||||
|
0x0BC6 |
3015 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII under frequency start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BC8 |
3017 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII under frequency reset/pick-up threshold percent
|
||||||||||||||||||||
|
0x0BCA |
3019 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI over frequency start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BCC |
3021 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI over frequency reset/Pick-up threshold percent
|
||||||||||||||||||||
|
0x0BCE |
3023 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII over frequency start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BD0 |
3025 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII over frequency reset/pick-up threshold percent
|
||||||||||||||||||||
|
0x0BD3 |
3028 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI under voltage start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BD5 |
3030 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI under voltage reset/Pick-up threshold percent
|
||||||||||||||||||||
|
0x0BD7 |
3032 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII under voltage start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BD9 |
3034 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII under voltage reset/pick-up threshold percent
|
||||||||||||||||||||
|
0x0BDB |
3036 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable over voltage transfer
|
||||||||||||||||||||
|
0x0BDC |
3037 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI over voltage start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BDE |
3039 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI over voltage reset/Pick-up threshold percent
|
||||||||||||||||||||
|
0x0BE0 |
3041 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII over voltage start/Drop-out threshold percent
|
||||||||||||||||||||
|
0x0BE2 |
3043 |
ALL |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII over voltage reset/Pick-up threshold percent
|
||||||||||||||||||||
|
0x0BE4 |
3045 |
3P/4P |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable voltage unbalance
|
||||||||||||||||||||
|
0x0BE5 |
3046 |
3P/4P |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SI unbalance threshold
|
||||||||||||||||||||
|
0x0BE7 |
3048 |
3P/4P |
R/W |
numeral |
FLOAT32 |
– |
TA |
– |
SII unbalance threshold
|
||||||||||||||||||||
|
0x0BE9 |
3050 |
4P |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable phase sequence warning
|
||||||||||||||||||||
|
0x0BEA |
3051 |
4P |
R |
ENUM |
ENUM |
– |
TA |
– |
Source phase sequence
|
||||||||||||||||||||
|
0x0BEF |
3056 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Source priority
|
||||||||||||||||||||
|
0x0BF0 |
3057 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Source usage
|
||||||||||||||||||||
|
0x0BF1 |
3058 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Auto transfer mode
|
||||||||||||||||||||
|
0x0BF2 |
3059 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
N to A confirmation transfer delay T2
|
||||||||||||||||||||
|
0x0BF4 |
3061 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
A to N confirmation transfer delay T6
|
||||||||||||||||||||
|
0x0BF6 |
3063 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Center-Off time delay T4
|
||||||||||||||||||||
|
0x0BF8 |
3065 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Generator start delay T7
|
||||||||||||||||||||
|
0x0BFA |
3067 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Generator stop delay T9
|
||||||||||||||||||||
|
0x0BFC |
3069 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable genset start fail warning
|
||||||||||||||||||||
|
0x0BFD |
3070 |
4P |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable neutral position wrong warning
|
||||||||||||||||||||
|
0x0BFE |
3071 |
4P |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Enable neutral loss warning
|
||||||||||||||||||||
|
0x0BFF |
3072 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Onload test timer T13 limited
|
||||||||||||||||||||
|
0x0C00 |
3073 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Onload test timer T13 time period
|
||||||||||||||||||||
|
0x0C02 |
3075 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Offload test timer T14 limited
|
||||||||||||||||||||
|
0x0C03 |
3076 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Offload test timer T14 time period
|
||||||||||||||||||||
|
0x0C05 |
3078 |
ALL |
R/W |
ENUM |
ENUM |
– |
TA |
– |
Test type from DI Test module config
|
||||||||||||||||||||
|
0x0C1B |
3100 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SI under frequency start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C1D |
3102 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SI under frequency reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C1F |
3104 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SII under frequency start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C21 |
3106 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SII under frequency reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C23 |
3108 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SI over frequency start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C25 |
3110 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SI over frequency reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C27 |
3112 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SII over frequency start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C29 |
3114 |
ALL |
R |
Hz |
FLOAT32 |
– |
TA |
– |
SII over frequency reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C2B |
3116 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SI under voltage start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C2D |
3118 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SI under voltage reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C2F |
3120 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SII under voltage start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C31 |
3122 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SII under voltage reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C33 |
3124 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SI over voltage start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C35 |
3126 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SI over voltage reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0C37 |
3128 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SII over voltage start/Drop-out threshold value
|
||||||||||||||||||||
|
0x0C39 |
3130 |
ALL |
R |
V |
FLOAT32 |
– |
TA |
– |
SII over voltage reset/Pick-up threshold value
|
||||||||||||||||||||
|
0x0DAB |
3500 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
Genset start failure alarm validity
|
||||||||||||||||||||
|
0x0DAC |
3501 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
Genset start failure alarm
|
||||||||||||||||||||
|
0x0DAD |
3502 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
External power supply presence validity
|
||||||||||||||||||||
|
0x0DAE |
3503 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
External power supply presence
|
||||||||||||||||||||
|
0x0DAF |
3504 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
Onload test failure alarm validity
|
||||||||||||||||||||
|
0x0DAF |
3504 |
ALL |
R |
– |
BOOL |
– |
TA |
1 |
Offload test failure alarm validity
|
||||||||||||||||||||
|
0x0DB0 |
3505 |
ALL |
R |
– |
BOOL |
– |
TA |
0 |
Onload test failure alarm
|
||||||||||||||||||||
|
0x0DB0 |
3505 |
ALL |
R |
– |
BOOL |
– |
TA |
1 |
Offload test failure alarm
|
||||||||||||||||||||
|
0x0DB1 |
3506 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Unexpected position alarm
|
||||||||||||||||||||
|
0x0FBD |
4030 |
ALL |
R |
numeral |
UINT32 |
– |
TA |
– |
Total Transfer count (no handle count)
|
||||||||||||||||||||
|
0x0FBF |
4032 |
ALL |
R |
numeral |
UINT32 |
– |
TA |
– |
Total Transfer failure count
|
||||||||||||||||||||
|
0x0FC1 |
4034 |
ALL |
R |
numeral |
UINT32 |
– |
TA |
– |
Too fast transfer counter
|
||||||||||||||||||||
|
0x0FD1 |
4050 |
ALL |
R |
numeral |
UINT32 |
– |
TA |
– |
Configuration changed count
|
||||||||||||||||||||
|
0x01389 |
5002 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Force to off function supported
|
||||||||||||||||||||
|
0x0138A |
5003 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Force to off status
|
||||||||||||||||||||
|
0x0138B |
5004 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Inhibit function supported
|
||||||||||||||||||||
|
0x0138C |
5005 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Inhibit status
|
||||||||||||||||||||
|
0x0138D |
5006 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Voluntary remote control function supported
|
||||||||||||||||||||
|
0x0138E |
5007 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Voluntary remote control status
|
||||||||||||||||||||
|
0x0138F |
5008 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Fire function supported
|
||||||||||||||||||||
|
0x01390 |
5009 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Fire status
|
||||||||||||||||||||
|
0x01391 |
5010 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Test status function supported
|
||||||||||||||||||||
|
0x01392 |
5011 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Test status
|
||||||||||||||||||||
|
0x01393 |
5012 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
HMI transfer function supported
|
||||||||||||||||||||
|
0x01394 |
5013 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
HMI transfer status (local control)
|
||||||||||||||||||||
|
0x01395 |
5014 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Comm control function supported
|
||||||||||||||||||||
|
0x01396 |
5015 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Transfer by comm status
|
||||||||||||||||||||
|
0x01397 |
5016 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Test result
|
||||||||||||||||||||
|
0x0144F |
5200 |
ALL |
R/W |
s |
FLOAT32 |
– |
TA |
– |
Load shedding time delay T8
|
||||||||||||||||||||
|
0x0176F |
6000 |
ALL |
R/W |
IEC870-5-4 |
DATETIME |
– |
TA |
– |
System time
|
||||||||||||||||||||
|
0x01773 |
6004 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Pole number
|
||||||||||||||||||||
|
0x01783 |
6020 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Product identifier
|
||||||||||||||||||||
|
0x01784 |
6021 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Vendor name
|
||||||||||||||||||||
|
0x0178E |
6031 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Product family
|
||||||||||||||||||||
|
0x01797 |
6040 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Product range
|
||||||||||||||||||||
|
0x017A1 |
6050 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Product model
|
||||||||||||||||||||
|
0x017A9 |
6058 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Product code CR num |
||||||||||||||||||||
|
0x017B1 |
6066 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Serial number PP-YY-ww-D-ll-xxxx |
||||||||||||||||||||
|
0x017BB |
6076 |
ALL |
R/W |
STRING |
STRING |
– |
TA |
– |
User application name "User app name" |
||||||||||||||||||||
|
0x017DB |
6108 |
ALL |
R/W |
STRING |
STRING |
– |
TA |
– |
Product capability "Product Capability" |
||||||||||||||||||||
|
0x017E7 |
6120 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
FW version xxx.yyy.zzz |
||||||||||||||||||||
|
0x017ED |
6126 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Hardware version xxx.yyy.zzz |
||||||||||||||||||||
|
0x017F3 |
6132 |
ALL |
R |
ENUM |
ENUM |
– |
TA |
– |
Current running image type
|
||||||||||||||||||||
|
0x017F4 |
6133 |
ALL |
R |
STRING |
STRING |
– |
TA |
– |
Vendor URL |
||||||||||||||||||||
|
0x02324 |
8997 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Enable transfer by comm
|
||||||||||||||||||||
|
0x02325 |
8998 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Check whether can do comm control
|
||||||||||||||||||||
|
0x02326 |
8999 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Comm control method
|
||||||||||||||||||||
|
0x02327 |
9000 |
ALL |
W |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Transfer by comm request
|
||||||||||||||||||||
|
0x02328 |
9001 |
ALL |
R |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Enable test by comm
|
||||||||||||||||||||
|
0x02329 |
9002 |
ALL |
W |
ENUM |
ENUM |
– |
TA (Frame 250, 630 and 800 only) |
– |
Test by comm request
|
||||||||||||||||||||
|
0x0270F |
10000 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Event log version 0-65535 |
||||||||||||||||||||
|
0x02710 |
10001 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Event log type 0-65535 |
||||||||||||||||||||
|
0x02711 |
10002 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Event log queue size (log number) 0-1000 |
||||||||||||||||||||
|
0x02712 |
10003 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Event log current log number in queue 0-1000 |
||||||||||||||||||||
|
0x02713 |
10004 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
Event log latest index 0-65535 |
||||||||||||||||||||
|
0x02714 |
10005 |
ALL |
R |
TI086 |
TI086 |
– |
TA |
– |
Event log content |
||||||||||||||||||||
|
0x09C3F |
40000 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
System log version 0-65535 |
||||||||||||||||||||
|
0x09C40 |
40001 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
System log type 0-65535 |
||||||||||||||||||||
|
0x09C41 |
40002 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
System log queue size (log number) 0-1000 |
||||||||||||||||||||
|
0x09C42 |
40003 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
System log current log number in queue 0-1000 |
||||||||||||||||||||
|
0x09C43 |
40004 |
ALL |
R |
numeral |
UINT16 |
– |
TA |
– |
System log latest index 0-65535 |
||||||||||||||||||||
|
0x09C44 |
40005 |
ALL |
R |
TI086 |
TI086 |
– |
TA |
– |
System log content |