DOCA0214EN–06

Power Connection Accessories

DANGER
Hazard of electric shock, explosion or arc flash
Ensure to prepare cables with correct stripping length specified in this section.
Failure to follow these instructions will result in death or serious injury.
WARNING
Hazard of fire
  • Use only specified wiring cross-section with the equipment and comply with the specified wiring requirements.
  • Tighten the connections to the specified torque values.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The power connectivity of the transfer switch can be improved by using power connection accessories. For the accessories connection of TransferPacT Active Automatic / Automatic / Remote 100– 250, 320– 630, and 800 A transfer switching equipment, refer to table in Insulation Rules.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?