DOCA0214EN–06

TPCDIO17 : Genset Start and Alarm

Wiring

Version 1

Version 2

NOTE: The G2 and G4 terminals are swapped on two versions. Please inspect the label on the rotary cover to locate the positions.

Terminal

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?