DOCA0214EN–06

Spreader

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • It is mandatory to install interphase barriers when spreaders are used.
  • It is mandatory to install insulating screen or custom made fiber insulating plate when spreaders are used.
Failure to follow these instructions will result in death or serious injury.

The spreaders are used on switches:

  • to increase the pole pitch and align the poles with circuit breaker poles or

  • to increase the clearance distance between phases or

  • to connect larger bars or lugs.

The spreaders are screwed on the switch using the screws delivered with the spreaders.

The table below provides the list of the spreader:

Switch

Number of poles

Spreader

Frame 250: 100–250 A

3P

LV431563

4P

TPSCON39(1)

4P

LV431564(2)

Frame 630: 320–630 A

Frame 800: 800 A

3P

TPSCON40

4P

TPSCON41(1)

4P

TPSCON68(2)

Frame 1600: 800–1600 A

3P

33622 / LV833622SP(1)

4P

33623 / LV833623SP(1)

(1) Spreaders for SI / SII power terminals only.

(2) Spreaders for load terminals only.

Spreaders are not compatible with the vertical connection adapter or cable-lug adapter on TransferPacT Active Automatic 800–1600 A transfer switching equipment.

For information on installation, consult the instruction sheets on Schneider Electric website:

  • TransferPacT Active Automatic / Automatic / Remote 100–250 A: GEX2525501

  • TransferPacT Active Automatic / Automatic / Remote 320–630 A: GEX2525601

  • TransferPacT Active Automatic / Automatic / Remote 800 A: BQT1751501

  • TransferPacT Active Automatic 800–1600 A: BQT7680301

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?