Active Automatic HMI with LCD Display
The Active Automatic HMI with LCD display of the switch matches to all extension accessories using TPCDIO15. It displays all logs and settings with password protection. It can also be extended with more advanced functions, such as communications with extension plus 24 V DC.
Active Automatic HMI Settings
|
Label |
Description |
Function |
|---|---|---|
|
1 |
LCD screen |
LCD screen for display |
|
2 |
ESC |
ESC button to cancel the selected option or return to the previous menu |
|
3 |
Up button |
Up navigation button for rolling up |
|
4 |
Down button |
Down navigation button for rolling down |
|
5 |
OK button |
OK button to confirm the selected option |